This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are planning to use TPS7H1101-SP device, In TPS7H1101-SP device we want to use the PCL pin to limit the output current.
we have below queries on the current limiter as listed below
we are looking for the device with internal OPAM, which senses the output current, when ever output current cross the threshold set, device should go to shut down based on sense.
Please let me know, do you need any other information.
Regards
Sunil B V R
Sunil,
When Over current limit is triggered, LDO output will go low/ shut down. However when the overload condition is removed output will recover.
Hello Ramesh Khanna,
Thanks for your reply.
As per the datasheet and your reply earlier, when ever over current limit triggers, output current is reduce to 50% of the current limit set. In that case still the shut down will happen, can you please share more details on this.
And also, can you please share the timining details, after how much time will the shut down will occur after the OCP triggers. And timinig details recover of the LDO when OCP is removed.
Regards
Sunil B V R