This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using TLK2711-sp, with an FPGA. The clock to the IC is given by the FPGA board it self. FPGA is Xilinx Kintex 7. Could you please help me out, if i can directly feed the clock from FPGA to the TLK2711, or do i need to add any jitter reduction IC or something like it. If yes then please suggest one.
Regards
Bhrugesh