Part Number: CD74AC175
REQUIRED ESD Sensitivity voltage HBM/CDM/MM ABOUT
other than above part no 2 more part number
REF5050MDREP
OPA2335AMJG
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD74AC175
REQUIRED ESD Sensitivity voltage HBM/CDM/MM ABOUT
other than above part no 2 more part number
REF5050MDREP
OPA2335AMJG
Hello Anjani,
I have the following information for the CD74AC175M
HBM passed 1kV
CDM didn't pass 500V which is the lowest increment it was tested at
MM passed 50V
Thanks,
Rami
PLease reply for Finish of Item (Gold /Pure Tin / Lead Free Tin)/any Other finshes pls mention. for part no. D74AC175, REF5050MDREP and OPA2335AMJG.
The lead finish is in the datasheet under the package option addendum and other material content can be found under the "Quality, reliability & packaging information" in the Ordering & quality section of the product page
The other two devices are not in this product folder. I would recommend reaching out to the produce line that handles them.
Thanks
Rami