Other Parts Discussed in Thread: SN74LVC2G17, UCC27517, SN55451B, SN75451B, UCC27517A-Q1

Hello,
I am using the buffer to drive optical transmitter which can require a current upto 96mA in worst case. As per the datasheet the current could be 32mA (i assume it means for each channel), so combining 3 output pins can give me 96mA. Is my understanding correct?
But the absolute maximum current is 100mA for ground pin. I could not find the details on maximum group current in ground pin over all temperature range.
Is it ok to go with the IC or you recommend other. Attached is the snapshot of schematic