Other Parts Discussed in Thread: SN74AVC24T245, SN74AVC16834
Team,
my customer is looking for a 16bit buffer similar to 74ALVC244, but in a package that is smaller than 50mm^2, eg a BGA package.
They need 0.8mm pitch.
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
my customer is looking for a 16bit buffer similar to 74ALVC244, but in a package that is smaller than 50mm^2, eg a BGA package.
They need 0.8mm pitch.
Best regards
There is no such device.
The nearest BGA device would be the SN74AVC24T245, a 24-bit transceiver with 0.65 mm pitch (45 mm²).
The smallest non-BGA device would be the SN74AVC16834 (TVSOP with 0.4 mm pitch, 72 mm²).