This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC541A: Is 5V on Vcc ok for part?

Part Number: SN74LVC541A
Other Parts Discussed in Thread: SN74AHCT541

Is 5V ok to be applied to pin 20 Vcc of SN74LVC541APWR? The recommended is 3.3V, but I see the max rating is 6.5V. So does that mean 5V Vcc is ok? That means the output will be 5V with input 3.3V when chip OE is enabled,

Thanks