This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC3G17: Signal Reflection (Output change of the buffer is reflected back to the input signal)

Part Number: SN74LVC3G17


Hi Team

We are using an SN74LVC3G17 as a buffer for 24Mhz Signal. The input of the buffer is about 3.3V peak to peak. In the output, we have kept a variable pot of about 0 - 500 Ohm. 

While we change the pot, We are also getting more reflection over an input signal. 100 Ohm is connected to another end. 

I still confuse output signal change in the buffer is reflected back to the input signal change