This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4504B: When VCC =3.3V, how Vih and Vil are determined?

Expert 3040 points
Part Number: CD4504B


Hi,

My customer want to use the case in Vcc=3.3V and Vdd=7.2V. According to related question, I konw Vcc=3.3V can work as well in customer usecase.

But in datasheet of DC4504B, there is no specification of VIL and VIH at Vcc=3.3V. 

Would you please tell us know the min/max of VIL and VIH at Vcc=3.3V?

Best Regards, NY

  • At 3.3 V, there are no guarantees (neither for VIH/VIL nor for the propagation delay).

    You can extrapolate from the other values and assume 0.3 × VCC / 0.7 × VCC. In any case, the other 3.3 V device should have no problems driving high-impedance CMOS inputs to near the rails.