This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXU0202: How to determine VIL, VIH, VOL, and VOH?

Genius 16510 points
Part Number: TXU0202

Tool/software:

Hi Experts,

For the IC with MPN# TXU0202DCUR, with the below requirements:
VCCA is 3.3V
VCCB is 5.0V
OE is pulled up at 3.3V through 4.7K RESISTOR

For the above condition, we want to know:
1. VIL and VIH for A1 Pin
2. VOL and VOH for B1Y Pin
3. VIL and VIH for B2 Pin
4. VOL and VOH for A2Y Pin

Regards,
Archie A.