Hello,
I am looking for an alternative of PCF8574 which is I2C based.
I need something that can work with SPI Interface (literally running out of pins to accommodate I2C).
I would like to receive an Interrupt (dedicated pin for INT) upon state change on the inputs. I have 7 Inputs in total so 8 bit Input expander should work. No outputs required.
Inputs are 0-3.3V levels. Mainly buttons.