This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am looking for an alternative of PCF8574 which is I2C based.
I need something that can work with SPI Interface (literally running out of pins to accommodate I2C).
I would like to receive an Interrupt (dedicated pin for INT) upon state change on the inputs. I have 7 Inputs in total so 8 bit Input expander should work. No outputs required.
Inputs are 0-3.3V levels. Mainly buttons.
In general, when you're running out of pins, I²C is the best solution because you can add devices with different addresses to an existing bus.
There is no SPI I/O expander. A parallel-in shift register like the SN74HCS165 can be SPI compatible, but it would require polling. Alternatively, program a separate MCU.
Thank you Clemens Ladisch that really helps.
Is there a way I can reduce some pin usage by using any of the communication master? Ex. I have 2 UART devices, few SPI devices, if I can replace these pins and combine with just one I2C line that would be helpful.
Is there any cost-effective MCU available with 20MHz+ speed which has at least 4 timers on the TI catalog?
I know Microchip has AVR ATTiny series - 2 for 1$. Is there any cost-effective solution from TI then I would like to use that instead of other options.
https://www.mouser.ca/ProductDetail/Microchip-Technology/ATTINY826-SFR?qs=sGAEpiMZZMv0NwlthflBi775BgPTl04svHdGpOcu4mo%3D
MCU has to be programmable using another MCU over UART/any other protocol.
There are many chips that can be accesses through I²C. Please specify what you want to replace.
This is a search for 20 MHz MCUs with four timers:
www.ti.com/microcontrollers-mcus-processors/microcontrollers/msp430-microcontrollers/products.html#p62=20;25&p2089=4;6
Clemens,
Thank you very much for the help here.
Jigar,
Please let us know what other questions you may have.
Regards,
Eric Hackett
I would like to use a MCU who I can program using my master MCU. Can you please suggest an option that has that capability right from the root?
I mean, MCU that we can program using another MCU over UART/SPI or any other protocol? And it's been widely proven as working model with examples for it available?
Most of the MSP430s I linked to above can be programmed with UART or I²C; see MSP430 Flash Devices Bootloader (BSL) or MSP430 FRAM Devices Bootloader (BSL).