Part Number: LSF0102
Other Parts Discussed in Thread: PCA9306, , TXS0102, TXS0101
Hello, I have to make a level translation from 3.3V to 5V on a 1-Wire bus (I have two 1-Wire lines on the board).
I have found several parts that seem suitable and I would like to make sure I make the right choice.
I believe LSF0102 should be good, otherwise TXS0102E seem to be a possible choice too. I have considered also PCA9306, even if it is targeted to I2C I believe it should work too, is that correct ?
Is it OK to use LSF0102 for this function ? Or is there a better option ?
Thanks,
Mihai