This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV165A: SN74LV165A: Schematic check

Part Number: SN74LV165A

S.pdf

Hi:

We need to read the electrical level of 80 output ports,We are not sure whether the connection is correct ,Please check Schematic !Thanks

  • The connections and power supplies are correct.

    The SER input of U13 must not be left floating. You can tie it to GND or VCC.

    If you have long traces, 33 Ω source termination resistors make sense in front of outputs like QH. But directly in front of inputs (CLK, SH/LD), they are pointless; if you do want source termination for these signals, there should be one resistor near the GPIO3/4 pin.

  • Thank you for your reply. The schematic will be modified as your recommended.