Other Parts Discussed in Thread: TPIC6B259, SN74LV163A, SN74HCS138
Hello forum,
I want to design a circuit that LED light sequencer. I want to turn on the leds one by one. I think of it as a floating signal circuit in a taillight design. In my design, I have 16 LEDs. Because of this, I selected 16bits counter CD4059AMG4.
I will apply 8V dc power. I need 50mA output current for each led.
I need to be able to determine the sliding speed of the leds and the current that will pass through the leds.
I hope that I can achieve this with the 555 IC, without using a microprocessor.
The datasheet of the integrated is not very clear, so I think it is the right decision to consult the forum. I have attached the datasheet as well.
I can do the functions I mentioned with this integrated, right? Could you help me?