This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC112A: Alternative with Lower Drive Strength?

Part Number: SN74LVC112A
Other Parts Discussed in Thread: CD74HC112

I need an alternative to the "LVC" logic family "112A" Dual FF device.
There is some Overshoot we need to limit - a lower drive strength P2P device should solve the issue without requiring PCB changes.

I am looking at the CD74HC112 as a candidate...could you confirm?
*Required Package is TSSOP

VOH

Vcc-0.5V(@1μA)
I believe this is a typo...VOH needs to be within Vcc - 0.5V over the rated output drive current (4mA?)

VOL

0.5V(@1μA)

Again, a typo...VOL means sinking current through the internal FET; thus a voltage drop...should be less than 0V + 0.5V for rated current (4mA?)

Output tr/tf

<5ns

*Larger than the LVC112A device

This is a little confusing, but I understand they need an output rise/fall time of "greater" than 5ns.

Propagation Delay

<15ns difference between tPHL and tPLH

The datasheet doesn't spec skew between tPHL and tPLH; it only specs the "Typ" propagation delay. Do we have any data comparing the TYP tPHL vs TYP tPLH? Are they within 15ns of each other (at 3.3V?)

Clock Input (VIH)

0.9Vcc

Clock Input (VIL)

0.1Vcc