Other Parts Discussed in Thread: CD74HC193
Hello E2E,
Our customer has a question about stretching the pulse of the SN74HC193, here are the details:
I am using 2 SN74HC193M in cascade to make a modulo 53 counter and the countdown is being clocked and the up is tied high. The terminal count down is connected to the parallel load inputs on both counters with the data inputs set to (msb first) 0011-0101 for a count of 53 but it is counting by 33 instead. The datasheet says that it should work with no external components but it does not work that way.
But just to clarify further I see that the minimum pulse width at the NOT Load input is 30ns but the terminal count down is only low for 26ns since the load function is async. How do I stretch the pulse?
I added a 150pf cap on the load inputs and now it is close it is dividing by 54.
The delay maybe too long and so it misses the first clock down.
The only thing is that the datasheet says they can be cascaded with no external components. BTW the TTL version works fine but the current drain is much too high for my application.
Regards,
Carlo