This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCH8T245: Datasheet Inquiry

Part Number: SN74LVCH8T245


Hi Team,

Could you please check our datasheet on page 13. Could you confirm if this is correct. Our customer had noticed this information and need to have an attention. 

8.1 Overview The SN74LVCH8T245 is an 8-bit, dual supply noninverting voltage level translator. Pins A1 through A4, and the control pins (DIR and OE) are referenced to VCCA, while pins B1 through B4 are referenced to VCCB. Both the A port and B port can accept I/O voltages ranging from 1.65 V to 5.5 V. The high on DIR allows data transmission from Port A to Port B, and a low on DIR allows data transmission from Port B to Port A. See AVC Logic Family Technology and Applications (SCEA006).

But as this is an 8 Bit part, shouldn't it rather be "Pins A1 through A8 (..)".Maybe this was copied from the 4-bit Version and overlooked, or am I mistaken?

Thank you for your advise. 

Best regards,

Jonathan