I have used a SN74LVC1G04 inverter to drive a small MOSFET through a resistor of 56Ohm. The peak current becomes 43mA for lees than 5ns, after which it drops within the limits defined in the datasheet. Which is 32mA.
Do I have to be concerned the device has a reduced lifespan or might lock up?