This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74VMEH22501A: Imin and Imax value in IBIS model

Part Number: SN74VMEH22501A
Other Parts Discussed in Thread: SN74LV14A

Hi Team, 

Since following thread is locked, let me open a new thread. 

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1093626/sn74vmeh22501a-undershoot-for-around-10ns/4053794#4053794

Since datasheet said "device can exceed -0.5V as long as IIK is lower than 50mA(SN74VMEH22501A) and 20mA(SN74LV14A) respectively", and Clemens said IIK can be estimated from IBIS model. Customer have 2 questions as following. 

1. Customer confirmed VMEH22501A_IO_3B pin, but it comes out I(min) is larger than I(max) when V=-0.665V, is it normal? 

2. Vpeak of undershoot = -0.54V in customer application, I is -30mA for worst case when VIN=-0.6V, so does it mean it is NG since exceeding abs. max rating which is 20mA? 

Thanks.

Regards,

Jo