This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4541B: CD4541B

Part Number: CD4541B

This part looks great for my application.  It is able to be retriggered and it has clock frequency division.  My biggest concern is that in the data sheet under features it states that the oscillator frequency range is DC to 100kHz but under the description portion it gives the equation for the frequency, resistor, and capacitor values and it states "Where frequency is between 1kHz and 100kHz".  So I need to know which requirement to follow either the CD4541B is capable of an oscillator frequency range of DC to 100kHz or it is only capable of an oscillator frequency range of 1kHz to 1000kHz.