This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4T125: Max output current for SN74LV4T125 and SN74LXC8T245

Part Number: SN74LV4T125

Dear Technical Support Team,

①Is the output current rating(Max) below due to the heat problem or the output voltage(VOH/VOL) cannot be maintained ?

② Are these specs for total channel output current or per channel?

■SN74LV4T125 

VOL/VOH: ±16mA(VCC=4.5V  VOH/VOL(MAX))

IO Continuous output current : ±35mA(Absolute Max)

Continuous current through VCC or GND:±70mA(Absolute Max)

■SN74LV4T125 

VOL/VOH: ±32mA(VCC=4.5V  VOH/VOL(MAX))

IO Continuous output current: ±50mA(Absolute Max)

Continuous current through VCC or GND:±200mA(Absolute Max)

Best Regards,

ttd