Other Parts Discussed in Thread: SN74HCS14
Page 4 of the data sheet says that the absolute maximum input voltage range is -0.5 to +6.5 volts. Note 2 says that the negative rating may be exceeded if the maximum input current rating of -50 mA is observed. Can the positive voltage rating also be exceeded if the current is limited to +50 mA?