This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Experts
Could you help me to find the guaranteed MIN and MAX VOH of SN74LVC08APWR at -40℃~85℃ when VCC and IOH as below? I can not find the curve or data of the VOH VS VCC.
1.MIN and MAX VOH when VCC 3.2V IOH 24mA
2.MIN and MAX VOH whenVCC 3.38V IOH 24mA
Thank you !
Hi SUN,
Please also see [FAQ] How do I determine the output voltage (VOH, VOL) or output current (IOH, IOL) of a CMOS logic device?.
If you have any remaining questions let me know.
Regards,
Owen