This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCH16T245: Effect of transient Loss of VCCA or VCCB

Part Number: SN74LVCH16T245


Hello,

I haven't seen anything about the effects of transient loss of a VCCA or VCCB power supply in the datasheet.

In our design, there may possibly be the loss of one of these voltages (3.3V and 1.8V) for a maximum time of 65ms.

Can you confirm that there will be no other effect than the possibility of having the outputs in an erroneous state and this regardless of:

  • the power supply configuration: - VCCA = 3V3 and VCCB = 1V8 or VCCA = 1V8 and VCCB = 3V3,
  • or the direction, from B to A or from A to B.

Thank you in advance,

Best regards

Pierre