This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
On 9.2 Typical Application, 6 pin Cext and 7 pin Rext/Cext are connected via a capacitor and then connected to VCC through a resistor.
But on Figure 1. Required Timing Circuit, Cext is connected to GND
Can the Cext be connected to GND? Is there any effect?
Best Regards,
Tom
Hi Tom,
The Cext pin is connected to ground internally, so you can connect it or not. It will not impact operation of the device.