This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Some similar devices directs that Cext pin should be tied to GND but our SN74LVC1G123 does not.
Why doesn’t it need to be tied to GND for SN74LVC1G123?
Thank you and best regards,
Michiaki
Designing with the SN74LVC1G123 Monostable Multivibrator says:
5.6 Can I connect the Cext pin to ground?
It is best to follow the datasheet recommendations. If your monostable multivibrator recommends not connecting Cext to ground, then do not connect it to ground.
In some monostable multivibrators the Cext pin is internally tied to ground, but in some it is not. If the datasheet is unclear and the information is required, use an ohmmeter to check the resistance between the two pins. If the resistance reads less than 1 Ω, it is safe to connect both to ground.
The functional diagram impluies implies that Cext is indeed connected to ground:
Hi Clemens,
Could you kindly advise the risk and concern if Cext was tied to GND ?
Some devices which have same function should be tied to GND.
Customer needs to make sure the risk and concern in the case of replacement to LVC1G123 from same function devices tied to GND.
Thank you and best regards,
MIchiaki