This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T126: automotive grade alternative

Part Number: SN74LV1T126
Other Parts Discussed in Thread: SN74LVC1G126-Q1, SN74AHCT1G126-Q1, TXU0101-Q1

Team,

Would like to check if we have Q-grade spin for SN74LV1T126, or any similar alternative, to suit customer's automotive design that requires AEC-Q100 solution. Thanks.

  • The SN74LVC1G126-Q1 has overvoltage-tolerant inputs and can be used to translate down.

    The SN74AHCT1G126-Q1 can be used to translate from 3.3 V to 5 V.

    If you want to translate up between other voltages, use the TXU0101-Q1, which requires two supplies.

    (There are more alternatives if you do not need an active-high OE input.)