This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T234: 26-Ω series resistor on A-side outputs of SN74AVC4T234

Part Number: SN74AVC4T234
Other Parts Discussed in Thread: SN74AVCBH164245

Hi,

Does SN74AVC4T234 have 26-Ω series resistor on A-side outputs as stated in the Features section of the datasheet?

The simulation result  with 10 in trace length, 50 MHz, Vcc = 1.5V using the IBIS model shows more than 0.5V overshoot at the load.

Thanks,

DH