This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74GTL2014: SN74GTL2014:Vol(max) value of B port output

Part Number: SN74GTL2014


Hi,

Could you let us know Vol(max) value of the SN74GTL2014 B port output(*1), when using iol=10mA(Vcc=3V).

On the datasheet, there is only a description of Vol(max) 0.4V, when the test condition is Iol=40mA(Vcc=3V).

*1:Connect DIR pin to VCC.

Thanks.
Makoto