This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: fall time spec

Part Number: TXS0102

Hi expert,

Customer used TXS0102 and have some questions about fall time measurement although so far no any issues. 

They used it for i2c 1.8V <> 3.3V. there is a spec in DS that A port fall time 4.3 ~ 6.4ns. 

Here is their measured result:

May I clarify with you if any concern about the result? Cause in i2c standard Fast Mode, fall time could be 20 × (VDD/ 5.5 V) ~300 ns as well.

Thanks,

Allan