This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245-EP: Using mixed voltage on VCCA port

Part Number: SN74LVC8T245-EP

Hi,

I'm trying to share SN74LVC8T245-EP across 1.8V/2.5V -> 3.3V conversion.

My application is similar to picture in Section 10.2 of the device datasheet. The direction is fixed portA (1.8V) to portB(3.3V).

But I also want to  use for example pin A8 as a 2.5V input and translate this across to pin B8 (3.3V).

Is this possible or will the input protection diodes start to clamp?

Thanks