This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXV0106-Q1: TI IBIS-AMI Model Request_TXV0106-Q1 & SN74AVC2T45-Q1

Part Number: TXV0106-Q1
Other Parts Discussed in Thread: SN74AVC2T45-Q1,

Please provide IBIS model and project details as follows

Device name of the model you are requesting :

  1. SN74AVC2T45-Q1
  2. TXV0106-Q1

Project details : 

For simulating a 100Mbps application between an ASIC and FPGA across a backplane including two connectors and 10 inches of total PCB trace.

  • Hi Liang,

    SN74AVC2T45-Q1

    You may use SN74AVC2T245 IBIS Model or any other IBIS model from the AVC family.

    TXV0106-Q1

    Please note that although the device is planned to be released to market soon, it is still under Accelerated Product Launch as of this time, but I have also gone ahead to submit a ticket for IBIS to be provided when released.

    However, I have performed multiple bench analysis on the TXV family and 100Mbps is of no concern for the device with typical capacitive loading.

    If further clarification is needed, please help estimate the total capacitive loading with the two connectors and 10 inches trace, thanks.

    Best Regards,

    Michael.

  • Thank you for your update regarding the device and its release status. I have noted that it is still under Accelerated Product Launch. I also appreciate your proactive action in submitting a ticket for IBIS data when it is released.