Hi,
customer need the failure rate to classify it in SN29500-2.
Which Table and Category of SN29500-2 is it?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
customer need the failure rate to classify it in SN29500-2.
Which Table and Category of SN29500-2 is it?
Regards, Holger
Hi Holger,
Here is the FIT rate for the DCKR package:
Otherwise please see the following two links for failure/reliability information:
If you need something more specific you'll have to request functional safety documentation on the internal forum.
Best,
Malcolm
Hi Malcolm,
here the “MTBF/FIT = 0.5 FIT” seems like a Reliability FIT data from field data, but customer needs the Functional Safety FIT rate based on SN29500-2.
The following info. is extracted from SN29500-2 Part 2 for SN74LVC1G125-Q1, pls help to confirm whether it is correct or not.
SN29500-2 Part 2: Expected values for integrated circuits.
Component Failure Rates per Siemens Norm SN29500-2 of SN74LVC1G125-Q1
Regards, Holger
Hi Holger,
Where are you seeing this table? Could you link the document?
I'd say probably that's correct but I'm curious where you're getting it from.
Best,
Malcolm
Hi Malcolm,
I will try to get more infos. The table is from the
Siemens Norm SN 29500-2, Edition 2004-12
|
Failure Rates of Components: Expected Values for Integrated Circuits. © Siemens AG 2004. For more information, see Entering Siemens Integrated Circuits.
|
It is not for free download.
Regards, Holger
Hi Malcom,
have you asked the system engineer for the functional safety FIT rate?
Regards, Holger
Hi Holger,
Please see attached for the FUSA document. Should have all the information you are looking for.