This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: TXS0108E

Part Number: TXS0108E
Other Parts Discussed in Thread: TMUX1511

Hi TI,

I'm testing logic circuit with TXS0108E, 1.8V to 1.8V .

While powerup, when OE pulled low, I see an unwanted 2.5ms High-level-pulse over B side,
when both sides A&B are pulled low with 100k-PD.
Leakage current is 2uA-max so the voltage should go up to 0.2V...

This phenomenon occurs on multiple lines, and causes bugs over power-control lines.

Do you have newer data-sheet (than july 2023) or errata?

BR,
Dudi