Part Number: CD4093B
I'm running into a problem with the PSpice model that I downloaded from the product page for the CD4093B.
I'll be the first to admit I'm not an expert when it comes to reading model syntax, but it appears to me that the subcircuit "LOGIC_GATE_2PIN_OD_LVC_2i_NAND_PP_ST_CD4093B" has 3 resistors with 1 terminal each tied to GND and the other side of the resistor floating.
Is there a newer version of the model available, or is there another potential explanation for this issue?
Screenshots included below.
Product Page Link:
https://www.ti.com/product/CD4093B#design-tools-simulation
Spice Model Download direct link:
https://www.ti.com/lit/zip/schm024
Full error text for future searchability:
ERROR(ORPSIM-15141): Less than 2 connections at node X_U17.XU1.NA1.
ERROR(ORPSIM-15141): Less than 2 connections at node X_U17.XU1.NB1.
ERROR(ORPSIM-15141): Less than 2 connections at node X_U17.XU1.NO1.
Relevant lines from CD4093.lib:
RDA1 NA1 GND 1e6
RDB1 NB1 GND 1e6
RDO1 NO1 GND 1e6