I am using the SN74LXC2T45QDCURQ1 IC with the following connections:
- VCCA connected to +3.3V
- VCCB connected to +1.8V
- DIR connected to GND (B to A)
Initial testing show correct translation. However, after further testing, A1/A2 don't reach +3.3V (measured either 0V or +2.5V - which are both incorrect).
What would cause this behavior?
Thanks.