Hi team,
I have seen that the MIN value of the High-level input voltage is 2V for 3.3V supply. Do we have a same device that has lower VIH than 2V with 3.3V supply (e.g. 1.7V)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I have seen that the MIN value of the High-level input voltage is 2V for 3.3V supply. Do we have a same device that has lower VIH than 2V with 3.3V supply (e.g. 1.7V)?
Hi Steve,
The only thing we would have is the 2-channel space-rated device:
SN54SC2T74-SEPRadiation Tolerant, Dual D-Type Flip-Flop With Integrated Translation datasheet
best,
Malcolm
Hi Steve,
Sorry I found a more suitable device that should work, but it's also 2-channel:
SN74LV2T74 data sheet, product information and support | TI.com
Best,
Malcolm
Hi Malcolm,
Thanks for your reply.
What is the difference between the 2V and below 2V devices? does they have different technology or focus on different application?