This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G14: Temperature dependence of threshold voltages

Part Number: SN74LVC1G14

Temperature dependence of threshold voltages of SN74LVC1G14DB
I measured with VCC = 3V
                            @ 0°C    @ 70°C
Positive Threshold Voltage  1.681V   1.675V
Negative Threshold Voltage  0.9V     0.938V
Hysteresis Voltage          0.781V   0.737V

So, the Hysteresis Voltage decreased around 5% from 0 to 70°C.

Can you confirm that the Hysteresis Voltage will always decrease with higher temperatures for all the SN74LVC1G14DB of all batches? Will it always be around 5% from 0 to 70°C?