Other Parts Discussed in Thread: TLV1811, TLV7211, UCC27527
Hi Clemens
Thanks for your prompt support in the past.
I've a few supplementary Q's, answers to which I could not gather from the Data Sheets.
Pl be good enough to reply at your convenience:
1) Configure it as a Schmitt Trigger ( Need a Positive Logic Schmitt Trigger unlike CD40106 )

Datasheet Shows Transition ( typ ) @7.5V ,& Vth+ As 11v max , Vth- as 4V Min . Should I Expect the Following?
Thresholds Rising Edge : 8.2 V Typ, 12 V Max
Falling Edge : Min 3.0 V , Typ 6.8 V
2) If i give a Triangular wave of 0V -15V- 0V at the input , What would be the Max Input Current @ transition point
Also, if a +15V Input appears when CD4050 is not powered, is the IC safe
3) Short pulse suppression circuit ( 1 uS Typ )

Do I need R2 (Current limiting at transition point ) & Clamping Diodes D1 &D2 . Max Freq. Is under 20 KHz.
4) Driving a 1nf Capacitor @ 20 kHz Max. Can I Use this:

Is CD4050B O/p capable of repeatedly charging 1nF at a Freq not exceeding 20 KHz
Thanking you in advance
BR
Varun