This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: set and application questions

Part Number: SN74LVC1G07

With SN74LV1G74 this film, the input is 100M CLK, and the original reference project is to output a 50M differential clock, but now there are 2 problems

First, the output differential mode, I understand that it should be Q to CLK_P, nQ to CLK_N

Second, I see that this film also has a single-ended connection, if SN74LV1G74 use single-ended output, what is the output CLK frequency? My current demand is to output a single-ended 50MHz CLK, but I don't see any configuration