Part Number: TXB0106
The TXB0106 is having the maximum continuous output current of 50mA in the absolute maximum ratings. I would like to get the info of the output current (typical) in the operating condition. The Vccb will be at 5V and Vcca will be 3.3V.