Tool/software:
hi,
Ultrasonic microscopy result:
We engaged an external lab to look at the defective components.
Result: Ultrasonic microscopy revealed delamination.
Red color arrow – delamination
Leadframe (Abb.9) and paddle (Abb.10)

Measurement:
All measurements were made with the following equipment:
· R&S HMP2020 Powersupply (940-0878-006)
· R&S RTB2004 Oscilloscope (940-1139-001)

Above picture shows a measurement of IC35, with the following signals:
Yellow: trigger signal
Green: IC35_Pin3 (output)
Orange: IC35_Pin2 (input)
Blue: IC35_Pin1 (input)
Since this IC is an AND-gate the output should switch to zero after Pin2 changed to zero, which it doesn’t do.
End customer try to file a FA request but the PIC ask me to search for advice from E2E to confirm.
Please advice.
Best Regards,
KPK
KPK