This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS11: Need Alternate of SN74HCS11DR without internal clamping diode

Part Number: SN74HCS11
Other Parts Discussed in Thread: SN74LVC11A, SN74LV11A

Tool/software:

Hello team,

I am looking for AND gate SOIC 14 package IC. which is having 3 AND gates.

I need pin to pin replacement of SN74HCS11DR IC.

Below are Specs :

1. Input voltage : 0V to 5V

2. Supply voltage : 0V to 3.3V

3. Schmitt trigger 

4. Package SOIC 14 - Pin to pin compatible with SN74HCS11DR

5 Without claming diode between VCC to input supply. 

we have found SN74LVC11A this part. In datasheet it is mentioned it is available in SOIC 14 package. but I am not able to find complete part number on digikey and mouser.

Can you please help me to get exact alternate of SN74HCS11DR without clamping diode.  

your quick support will be appericiated. 

Thanks and Regards

Shubham bajpeyee

+91 8484 860 263