SN74HCS574: Multi Stage Frequency Division using Octal D Flip Flop

Part Number: SN74HCS574
Other Parts Discussed in Thread: SN74HCS74

Tool/software:

Hello E2E Community,

We plan to use a pulse output (88kHz) sensor in our system, but need to reduce the frequency of these pulses from 88kHz to 22kHz & plan to use D Flip-Flop for this pulse frequency reduction.

Kindly guide which device with more than 2 D Flip Flops can we use for this use case?

Ideally we would like to have a Schmitt trigger inputs (HCS family). But I noticed Quad & above devices do not have complementary outputs, any suggestions how to achieve more than f/4 frequency reduction in same device from TI Portfolio?

Your insights on the portfolio options shall be very helpful.