Other Parts Discussed in Thread: LSF0204, TXU0202, TCA9800, TXU0102
Tool/software:
Hi team,
Customer met one issue which need your help. You can find the schematic, description and waveform as below.
Description:
After running under -40C, we found 4 pcs input low level signal become abnormal that the input signal from A1 channel(PIN 2) cannot be pulled a normal low level. We can still find about 0.837V when A1 logic is low, see picture 1 for waveform(CH1=A1 channel, CH2=A2 channel). After de-soldering PIN 12 & 13 to leave it open(disconnect output), you can find that the low level signal is back to normal, see picture 2 for waveform.
Picture 3 is the normal input waveform before putting device run at -40C, low level signal shows normal.
Questions:
1. Output load equivalent capacitive value is about 60pF. Is this phenomenon related to the Cload requirement? What is the output capacitive load capability of LSF0204-Q1?
2. Do you know why and how low temperature cause this abnormal?
Picture 1 abnormal waveform
Picture 2 input waveform after disconnect output
Picture 3 input waveform before put it at -40C
Schematic: each input and output channel have 2Kohm pull up resistor which not show in the screenshot.
Thanks!
Ethan Wen