This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I am looking for a SPI level shifter however I need one which can handle multiple devices.
Ideally would be TXU0304 but with 6 GPIO however I noticed that you don't offer this.
Which alternative is closest to the one mentioned above? LSF0108?
Hi Revky,
You may also use the TXV family for GPIO with more channels. See TXV0106 or TXV0108. See https://www.ti.com/lit/po/scea118/scea118.pdf?ts=1721834839275&ref_url=https%253A%252F%252Fwww.google.com%252F for additional GPIO recommendations, thanks.
Best Regards,
Michael.
Use TXU0304 + TXU0102 (or TXU0104 + TXU0202), or 2× TXU0304 to simplify the BOM.
If you want a single chip, you have to use an unbuffered translator like the LSF0108 or TXS0108E.