Other Parts Discussed in Thread: TXS0206A,
Tool/software:
Hi expert,
Customer is looking for a level shift solution 1.8V <> 3.3V for SDIO with 50Mhz clock rate. They used to use TXS but failed and pass with TXB. What they learnt it might because of the internal pullup of TXS cause SDIO_CLK don't need pullup but data and cmd do.
But what I see the DS of TXB, it looks weird to me TXB can only support up to 30Mhz. (TXS can only support up to 35Mhz for 1.8V <> 3.3V).

We discussed about TXS0206A but the pitch is too small and need extra cost for pcb assembly so the plan was rejected.
Now they consider more flexible LSF0108 with external pullups which is also p2p with TXB. However, I see the thread "LSF0108 translation 1.8V/3.3V@100MHz", we don't recommend LSF for SDIO.
I'm confused that the reason we put the figure 1 in LSF0108 DS is the use case is still acceptable or not recommended at all?

Customer prefer to consolidate multi-chips into single solution for 6ch SDIO CLK, CMD, and DATAn(4bit). Would it be doable and could you please advise a proper solution?
p.s. there is actually another need for UART and GPIO level shift. So it's preferable for customer if LSF0108 can also be used for easier BOM control.
Regards,
Allan