Part Number: LSF0102
Tool/software:
Hi team,
Although the LSF0102 supports frequencies up to 10 MHz, the waveform is dull even with 2.4 MHz signals, as shown below, and customer suspect the pull-up resistor is the cause.
1. The LSF0102 can be used with either push-pull or open train, but what determines this switching?
If there is a pull-up resistor, does it operate in open-drain mode, and if not, does it operate in push-pull mode?
2. I checked the data sheet for the proper value of the constant of the pull-up resistor, and the description is as follows.
Based on the statement “TThe device driving the low state at 0.175V must sink current from one or more of the pull-up resistors and maintain VOL,” I do not understand what specific resistor value should be selected.
What specific calculations are necessary?
3. Is it sufficient to determine the upper limit of the pull-up resistor based on the required current value for the IC to be connected? Are there any particular specifications for LSF0102?


Regards
Hayashi