This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AVC logic family dynamic output control function

Other Parts Discussed in Thread: SN74AVC16T245, SN74AVCA164245

Hi,

I'm curious about the dynamic output control (DOC) circuit discussed in the AVC technology guide SCEA006A.

My question is: do all members of the AVC family have this function? Only a few devices in the family have data sheets that mention it.

For instance -- I'm trying to select a 16-bit level-translator / buffer for my project. The SN74AVCA164245 datasheet mentions the DOC function, while the newer SN74AVC16T245 does not.

The SN74AVC16T245 otherwise seems to be a "better" version of the SN74AVCA164245 -- reduced tpd, reduced leakage, but I'd like to use the DOC circuit if possible.

 

In my application, I'm using the translator/buffer to drive a fairly long line (about 15cm), at a maximum of around 25 MHz (it's an HPI port on a TI DSP). As the DOC circuit has variable impedance, can anyone give some guidance as to the controlled impedance I should shoot for on the trace to minimize reflections? Ie. what is the nominal driver impedance in the high-drive / low-drive states?

 

Thanks for the help,

- Craig