I am using an LSF0108 to translate between 1.8V to 3.3V
On the 1.8V side is connected to WL1837 WiFi card - SDIO interface (CLK, CMD, D0-D3)
On the 3.3V side is connected to AM5716 processor to mmc3 interface
I can't get it work for frequencies greater than 10 MHz
What are the correct pull-up values for both sides?
Every pin need pull-up?
Right now i have 1kOhm pull-ups on 3.3V side and 500 Ohm pull-ups on 1.8V side